Can an alarm be triggered on the ALM2064 when not connected to a CM6800 Series Matrix?

Issue

Can an alarm be triggered on the ALM2064 when not connected to a CM6800 Series Matrix?

Product Line

Pelco Matrix

Environment

ALM2064
CM6800 Series Matrix

Cause

The ALM2064 is an alarm interface unit that must connects directly to the System 6800 matrix switcher/controller.

Resolution

The ALM2064 will not function as a standalone system; it must be connected to a CM6800 Series Matrix.