What are the required UTP (Unshielded Twisted Pair) connections on my ICS Series camera?

Issue

What are the required UTP (Unshielded Twisted Pair) connections on my ICS Series camera?

Product Line

Pelco Cameras

Environment

ICS Series camera

Cause

Installation - Use UTP for video output signal.

Resolution

The ICS110-CW Series camera offers support for unshielded twisted pair (UTP). The UTP video output signal is 1 Vp-p differential into a 100-ohm load. The unit uses active UTP At a minimum, UTP requires Cat 5, 100-ohm twisted pair cable. The maximum UTP wiring distance is 3,000 ft (914 m).

Use the :

Blue wire = Video +

Gray wire = Video -