Can I add 3 CM9760-CXTA Coaxitron Translators to a single sercom port on the CM9700-CC1 CPU controller?

Issue

Can I add 3 CM9760-CXTA Coaxitron Translators to a single sercom port on the CM9700-CC1 CPU controller?

Product Line

Pelco Matrix

Environment

CM9760-CXTA Coaxitron Translators
CM9700-CC1 CPU

Cause

Increase the interface unit for coaxitron-capable receivers for command and control functions.

Resolution

No. You can only add 2 CM9760-CXTA Coaxitron Translators per port with a total of 32 addresses when connecting to the CM9700-CC1 CPU controller.