What is the command for deleting temporary files from the CM9760-CC1 CPU controllers C:\97XX DOS directory?

NOTICE

POTENTIAL FOR DATA LOSS.
The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.

Issue

Unwanted temporary files in the C:\97XX DOS directory.

Product Line

Pelco Matrix

Environment

CM9760-CC1 CPU controllers

Cause

Delete temporary files to free space.

Resolution

Temporary files are created from executing live updates from the Pelco System Manager to the CM9760-CC1 CPU controller. These files should be purged on a regular bases when convenient.
The following commands will delete the temporary files.
DEL {FILENAME}.??0
DEL {FILENAME}.??1
DEL {FILENAME}.??2