How many operator keyboards can be added to the CM9740-CC1 Central Processing Unit?

Issue

How many operator keyboards can be added to the CM9740-CC1 Central Processing Unit?

Product Line

Pelco Matrix

Environment

CM9740-CC1
CM9760-KBD keyboard

Cause

Add additional operators to the CM9760-CC1 CPU (Central Processing Unit)

Resolution

The CM9740-CC1 Central Processing Unit has 16 sercom ports, any of these 16 ports can be programmed for a CM9760-KBD Intelligent Keyboard.