What protocol does the CM9760-KBD put out in Direct Camera Control mode?

Issue

What protocol does the CM9760-KBD put out in Direct Camera Control mode?

Product Line

Pelco Matrix

Environment

CM9760-KBD keyboard
 

Cause

Need to know the CM9760-KBD Direct Mode protocol to configure the camera protocol.

Resolution

When configured for Direct Camera Control the CM9760-KBD output is Pelco P protocol with EVEN Parity.

View Lessons Learned Article LL#9747 for programming settings. Parity Change for PTZ control of Spectra IV or New Esprit ES40/41 requires Parity of NONE.