Can 3rd party DVR's and other controllers access Pelco PTZ camera 95 preset menu?

Issue

Can 3rd party DVR's access the Spectras 95 preset menu?

Product Line

Pelco Cameras

Environment

Spectra III Series
Spectra IV Series
Third-party DVR

Cause

Access Spectra menu to configure camera settings.

Resolution

The command to enter Spectra menus is 95 Preset. Unfortunately, most 3rd party Controllers do not support this function. Contact the 3rd Party technical support for verification if the 95 Preset option is available for your controller.