Which DVR/HVR units does the DX Series Client support?

Issue

Which DVR/HVR units does the DX Series Client support?

Product Line

Pelco Video Management

Environment

  • DX Series Client
  • DX8100 / DX8000
  • DX4800(HD) / DX4700(HD)
  • DX4600 / DX4500
  • DX4100
  • DX4000

Cause

Product Compatibility

Resolution

The supported DVR/HVRs that the DX Series Client supports are:

  • DX8000/DX8100 Series
  • DX4700/DX4800(HD) Series
  • DX4500/DX4600 Series
  • DX4104 Series
  • DX4000 Series (Only works with DX Series Client v2.0.1.0036)

To see the DX Series Client supported features click HERE.