The CM9760-KBD Intelligent Keyboard displays SYSTEM 9760 or SYSTEM 9700

Issue

Why the LCD on the CM9760-KBD Intelligent Keyboard displays ""SYSTEM 9760" or "SYSTEM 9700"?

Product Line

Pelco Matrix

Environment

CM9760-KBD keyboard

Cause

The message on the CM9760-KBD is the logon prompt to a CM9700 Series Matrix. 

Resolution

"SYSTEM 9760" or "SYSTEM 9700" is the logon prompt for a CM9760-KBD Intelligent Keyboard connected to a CM9700 Series Matrix. To logon, enter a valid 4-digit operator PIN number.