Run a sequence on a CM6700 or CM6800 Series Matrix Switcher using the NEXT and PREV keys on the KBD300A keyboard.

Issue

How do I run a sequence on a CM6700 or CM6800 Series Matrix Switcher using the NEXT and PREV keys on the KBD300A keyboard?

Product Line

Pelco Matrix

Environment

CM6700 / CM6800 Series Matrix Switcher
KBD300A

Cause

View cameras in ascend or descend orders.

Resolution

The following procedure applies to KBD100, KBD200 and KBD300A Keyboards connected to either a CM6700 or CM6800 Series Matrix Switcher.

To run a sequence in count up numerical order:

  1. Hold down the NEXT key for 2-3 seconds and let go.
  2. Verify the SEQUENCE starts.
    NOTE: Cameras will start sequencing in a count up numerical order.

To run a sequence in count down numerical order:

  1. Hold down the PREV key for 2-3 seconds. 
  2. Verify the SEQUENCE starts.
    NOTE: Cameras will start sequencing in a count down numerical order.

To run sequence #1 or sequence #2: ( NOTE: this type of sequence is normally used when selected cameras are chosen in the sequence program).

  1. Press the sequence number (1 or 2).
  2. Press and hold down the NEXT key for 2-3 seconds.
  3. Verify the sequence starts.

To stop a sequence

  1.  Press the HOLD button for approximately 7 seconds and release.
  2.  Recall camera by pressing 1 then CAM.   
  3. Verify the sequence has stopped.