How many free IP camera licenses does the Digital Sentry NVs and DSSRV systems include from the factory.

Issue

How many free IP camera licenses does the Digital Sentry NVS include now that the Digital Sentry SRV includes 8 free IP camera licenses.

Product Line

Pelco Video Management

Environment

  • Digital Sentry NVs
  • DSSRV / DSSRV2
  • Digital Sentry XPress
  • Digital Sentry Realvue
  • Digital Sentry DS100
  • DS

Cause

Product Specification

Resolution

DS NVs
DS NVs models includes 4 IP Licenses for Pelco and/or Third-Party IP Cameras/Encoders.

Source : DS NVs Product Specification

DSSRV / DSSRV2
DSSRV models include 8 IP Licenses for Pelco and/or Third-Party IP Cameras/Encoders.
Note: Analog cameras on the ENC5416's or ENC5516's do not require IP licenses.


Source: DSSRV Product Specification

DS Legacy HVR
DS Xpress, DS Realvue Xpress, DS1000 models running software versions 4.3 - 7.2.30 include 4 IP Licenses for Pelco cameras only. 
Note:
Third-Party IP Cameras/Encoders will require a purchased license.
 

Source: DS Xpress Product Specification
 

Related Articles:

How do I update the IP camera license for a Digital Sentry?