How do I change the multi display on a the AUX monitor output of the MasterControl DVXi?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I change the multi display on a the AUX monitor output of the MasterControl DVXi?

Product Line

Pelco Video Management

Environment

  • MasterControl
  • DVXi
  • DVXe
  • DVX500

Cause

Custom layout desired.

Resolution

CONFIGURING MULTI-CAMERA OUTPUT

The MultiOut tab allows you to configure the multi-camera video output available on all DVXi systems. Six multi-camera configurations can be displayed on external monitors: 2x2, 3x3, 4x4, 7-camera, 10-camera, and 13-camera (along with a single-camera option). Multiple views can exist for each of the configurations. Default configurations initially display cameras in order of their input number, but you can change this.

You can also create new views using any of the multi-camera configurations. To create a multi-camera view, complete the following steps:

  1. Select one of the six multi-camera configuration buttons. This displays a model of the configuration that shows its arrangement of video windows.
  2. Select a camera from the Camera Name list and drag it to a video window in the configuration model. Repeat for each camera that you want displayed in this multi-camera view.
  3. Click Save View and name the view.

To change an existing view (including a default view), select it from the View list and perform step 2 from the preceding instructions. To delete a view, select it from the View List and click Delete View.


Information on viewing video on the AUX monitor output, refer to article: How do I view video on the AUX monitor output for the MasterControl DVX system?