What is the wire awg size and length used for the Analog wiring harness of the IPSXM-7 or -2 Exsite Power Module?

Issue

What is the wire awg size and length used for the wiring harness of the IPSXM-7 or -2 Exsite Power Module?

Product Line

Pelco Cameras

Environment

IPSXM-7 or -2

Cause

Product Specification

Resolution

  • The IPSXM-7 and IPSXM-2 are factory assembled with 22 awg wire at a length of 84 inches.
  • The Power wires for both the IPSXM models are 16 awg wire at 84 inches.
  • Subtract at most about 1 foot in length for internal wiring assembly. This would bring length total out of base to 6 foot.
  • The coaxial cable is an RG174 at 8 foot per assembly. Out of base would be 7 foot.