Power input connection for the EH3512-2 Series Enclosure

Issue

Where is the location to attach power wires on the EH3512-2 Series Enclosure?

Product Line

Pelco Cameras

Environment

  • EH3512-1 (requires separate power for 12VDC/24VAC camera)
  • EH3512-2
  • EH3512-3 (requires separate power for 12VDC/24VAC camera)
  • EH3515 Series

Cause

Need to find the power connection strip in the EH3512-2 enclosure to apply power to.

Resolution

There is a terminal connection strip on the inside of the EH3512-2 Series Enclosure, connect your 24VAC to pins 1 and 2.

Schematic of Internal PCB