Can the CM9502-KBD control a Spectra III or Spectra IV in direct mode?

Issue

Can the CM9502-KBD control a Spectra III or Spectra IV in direct mode?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM9502-KBD Keyboard
  • Spectra III Series
  • Spectra IV Series

Cause

Use CM9502-KBD keyboard to control the Spectra without the use of another devices.

Resolution

The CM9502-KBD does not provide direct camera control. Options to consider are the CM9760-KBD Intelligent Keyboard or the KBD300A Universal Keyboard for RS422 Pelco P protocol control.

See LL#13440 for compatible systems with the CM9502-KBD