Clear and re-program a pattern on the Spectra III and IV Series

Issue

How do I clear and re-program a pattern on the Spectra III and IV Series?

Product Line

Pelco Cameras

Environment

Spectra III Series
Spectra IV Series
KBD300A Keyboard

Cause

Set a new pattern for the Spectra dome.

Resolution

Clear program Pattern:

Option 1:
On the keyboard perform the following action:

  1. Press 95 then press and hold Preset for several seconds until Camera menu appears.
  2. Tap down to "DOME SETTINGS".
  3. Press IRIS OPEN.  
  4. Tap to "CLEAR".
  5. Press IRIS OPEN
  6. Tap to "CLEAR ALL PATTERNS".
  7. Press IRIS OPEN. All program pattern cleared.  


Option 2:
On the keyboard perform the following action:

  1. Press 95 then press and hold Preset for several seconds until Camera menu appears
  2. Tap down to "DOME SETTINGS".  
  3. Press IRIS OPEN.
  4. Tap to "PATTERNS"
  5. Press IRIS OPEN.
  6. Tap to "CLEAR PATTERN". 
  7. Press IRIS OPEN. The pattern number you called up deleted.

Program Pattern:

On the keyboard perform the following action:

  1. Press 95 then press and hold Preset for several seconds until Camera menu appears
  2. Tap down to "DOME SETTINGS".  
  3. Press IRIS OPEN 
  4. Tap to "PATTERNS". 
  5. Press IRIS OPEN.
  6. Tap to "PROGRAM PATTERN".
  7. Press IRIS OPEN.
  8. Move the dome to the start point.
  9. Press IRIS OPEN
  10. Move the dome to the desire pattern.
  11. Press IRIS OPEN. Pattern saved.