Will the CM9760-SER-32 rocket port card work with a CM9780 Series Matrix Switcher?

Issue

Will the CM9760-SER-32 rocket port card work with a CM9780 Series Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM9760-SER-32
CM9780 Series Matrix Switcher

Cause

Product compatibility

Resolution

Yes, the CM9760-SER-32 rocket port card part number has been updated to CM9700-SER-32. The 32 channel RS422 interface card may be used in all CM9760 and CM9700 Series Central Processing Units.