How do I save the display on the CCC5100H-6 Series SIMD Digital Color Camera?

Issue

How do I save the display on the CCC5100H-6 Series SIMD Digital Color Camera?

Product Line

Pelco Cameras

Environment

CCC5100H-6 Series

Cause

Screen capture and save the current view of the CCC5100H-6

Resolution

To save the Display on the CCC5100H-6 Series SIMD Digital Color Camera.

1. Go into Profile, change to active. 

2. Change Default to Custom 1

3. Save As Custom 1

4 Go into Camera Display and change the display to a new setting.

5. Then Go back into Profiles and save as custom 1 again 

6. Exit and the display will have changed and also saved.