How do I expand a CM6800E-48x8 Matrix Switcher to 96x16?

Issue

How do I expand a CM6800E-48x8 Matrix Switcher to 96x16?

Product Line

Pelco Matrix

Environment

CM6800E-48x8 Matrix Switcher

Cause

Increase current Matrix system 48 cameras and 8 monitor to 96 cameras and 16 monitors.

Resolution

Two CM6800E-48x8 Matrix switchers can be stacked to create a CM6800E-96x16 system allowing full crosspoint switching of 96 cameras to 16 monitors.  This configuration requires two CM6800E-48x8 Matrix Switchers and a cabling kit (PN:  CM6800E-KIT).

Refer to the Pelco CM6800E-48X8 Matrix Switcher Installation/Operation manual for full installation and programming details.

Note: Keyboards, Genex multiplexers, and other peripheral devices can only be connected to the main unit. The expansion unit can only support cameras, PTZ receivers, monitors, local alarms, and local relays.