Error message:Inetw performed an illegal operation, causing an invalid page fault in mfc42.dll.

Issue

After Entering Password, an error message appears:"Inetw performed an illegal operation, causing an invalid page fault in mfc42.dll."

Product Line

TAC I/NET

Environment

I/NET

Cause

Error in the Registry

Resolution

Warning! Improper use of regedit may damage PC’s operation.

Using regedit, delete the tool bars from the registry. The I/NET toolbars are rebuilt automatically.

  1. Shut down I/NET
  2. Start the registry editor
  3. Go to Hkey_Current_User\Software\CSI-Controls Systems International\InetW\Toolbars
  4. Delete all Tool Bar entries