How do I determine the Esprit ImagePak includes a wall mount?

Issue

How do I determine the Esprit ImagePak includes a wall mount?

Product Line

Pelco Cameras

Environment

Esprit ImagePak

Cause

Require wall mount for installation site.

Resolution

The mounting option is recommended to be predetermined prior to ordering esprit. The ImagePak uses a lettering scheme towards end of the number structure to determine mount option supplied. Example:

ES31CBW35-5W     The last letter "W " designates the wall mount option. "W" signifies the EWM wall mount option.
ES31CWB35-5N        The last letter "N" designates the pedestal mount option.  "N" signifies the EPP pedestal adapter plate.

Optional mounting adapters for corner, pole, and parapet applications can be found in the Esprit Product Specification Sheet.