Pelco PTZ protocols supported by the CM6800 Matrix Series

Issue

What Pelco PTZ protocols does the CM6800 Matrix Series support?

Product Line

Pelco Matrix

Environment

  • CM6800 Matrix Series

Cause

  • PTZ protocol options

Resolution

The CM6800 Matrix Series supports the following Pelco Protocols for PTZ control through system programming:

  • EXT COAX       Extended Coaxitron (32 Bit).
  • STD COAX      Standard Coaxitron (15 Bit).
  • Pelco P             RS-422 Two Wire Control.
  • Pelco D             RS-422 Two Wire Control.

Related articles:

Program the CM6800 Series Matrix for RS422 control of PTZ cameras.

 How to program the CM6800 for RS485 PTZ control?

Can the CM6700/CM6800 Matrix Switchers control 3rd party PTZ cameras?