How many audio channels does the DSSRV support?

Issue

How many audio streams can be recorded/connected to the DSSRV recorder.

Product Line

Pelco Video Management

Environment

DSSRV
ENC5416

Cause

Supported audio connection limit

Resolution

The DSSRV supports audio recording either using the ENC5416's with analog cameras or using the built in audio support with Sarix IP cameras.

Total support = 128 audio streams.

Analog (ENC5416's) = 64
IP (Sarix IP cameras) = 64 - *128


*128 if only Sarix IP cameras are connected with no ENC5416, must not exceed the 128 limit.  Also must not exceed the maximum throughput of a DSSRV which is 280Mbps including client connections.