NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
What PTZ protocol is used when connecting a DS Xpress to a CM9760-CXTA Coaxitron translator?
Product Line
Pelco Video Management
Environment
- Digital Sentry
- DS XPress
- DS RealVue Xpress
- DS1000
- DS Desktop
- CM9760-CXTA
Cause
Recommended configuration to make the communication between a DSSRV or DSXPress and the CM9760-CXTA.
Resolution
DSXPress and CM9760-CXTA
Connection illustration:
-
Make all necessary connections with system powered off.
Note: Looping video to three or more devices can cause PTZ control to malfunction, when configuring for the first time setup DS system and CM9760-CXTA as illustrated.
Note: DS RealVue and DS1000 are labeled TX+/- on the back of the unit.
-
Change the Dip switch on the CM9760-CXTA.
-
Connect the Data cable between the CM9760-CXTA to DS system.
- Configure DS Admin for Pelco D No Parity.
Related Articles: