Can a keyboard be restricted control only a specific monitor on a CM9700 Series Matrix.

Issue

Can a keyboard be restricted control only a specific monitor on a CM9700 Series Matrix.

Product Line

Pelco Matrix

Environment

CM9700 Series Matrix

Cause

Configure Keyboard Group to restrict access to specific monitor.

Resolution

Keyboard Groups may be created and assigned to monitors using CM9700 System Manager.  Only keyboards which are assigned to the Keyboard Group will be able to access and control the display of the monitor.  Keyboards that are not members of a monitors assigned keyboard group will receive a Monitor Denied message when attempting to select the monitor. 

The default Keyboard Group assigned to all monitors is All Keyboards.

For more information refer to page 49, "How to Create a Keyboard Group" of the CM9700 System Manager Software Guide.