Clear the presets stored on a Spectra III or Spectra IV Series Dome camera.

Issue

How do I clear the presets stored on a Spectra III or Spectra IV Series Dome camera?

Product Line

Pelco Cameras

Environment

Spectra III Series
Spectra IV Series

Cause

Clear stored preset and re-configure new preset settings.

Resolution

  1. Access the cameras on screen menus by calling Preset 95.
    Refer to Lessons Learned article "Access Spectra main menu (Preset 95)" for instructions on programming preset 95 for Pelco's controllers
  2. Select , the Dome Settings submenu appears.
  3. Select , the Presets submenu appears.
  4. Select Clear Preset and press the Iris Open button.