What are the power recommendations for the Spectra IP mini?

Issue

What are the power recommendations for the Spectra IP mini?

Product Line

Pelco Cameras

Environment

Spectra IP Mini

Cause

Installation

Resolution

Power requirements:
Input Voltage/Amps 18 to 30 VAC, 24 VAC nominal; 0.75 A, 50/60 Hz
nominal Input Power 18 VA
PoE IEEE 802.3af class 3