Default IP address for the NET300T and the NET300R?

Issue

What is the default IP address for the NET300T and the NET300R?

Product Line

Pelco Transmission & Power

Environment

PelcoNet NET300T
PelcoNet NET300R
PC computer

Cause

Configuration - Test connection between PC and PelcoNet.

Resolution

The default IP address for the NET300T is 10.0.0.1 and for the NET300R it is 10.0.0.2.