Can I turn off the Azimuth label on the Esprit Camera Series?

Issue

Can I turn off the Azimuth label on the Esprit Camera Series?

Product Line

Pelco Cameras

Environment

Esprit Series

Cause

Remove the Azimuth label on the monitor screen.

Resolution

Yes. Follow these steps:
 

1.  Use 95 preset set to open menu of Esprit.
2.  Move to other and hit open Iris
3.  Use joystick to move to AZ/EI Direction hit open iris
4.  Move joystick up or down look for off hit open iris
5.  Move joystick to Direction hit open iris
6.  Move joystick up or down look for off hit open iris
7.  Move joystick to Zoom and hit open iris
8.  Move joystick up or down look for off hit open iris
9.  Move to exit and hit open iris.