Access the Spectra Dome menu through the CM6800 Matrix Switcher using the KBD300A/KBD200A keyboard

Issue

How to access the Spectra Dome menu through the CM6800 Matrix Switcher

Product Line

Pelco Matrix

Environment

  • CM6800 Matrix Switcher (All Version)
  • KBD300A keyboard (All Version)
  • KBD200A Keyboard (All Version)
  • CCTV Monitor

Cause

Access Spectra Dome to configure settings.

Resolution

  1. Enter 95
  2. Hold PRESET for 2 seconds.
  3. Preset Label menu will appear on monitor.
  4. Move down to the Set and it will start flashing.
  5. Move joystick to right or press right button 
  6. Camera menu will open

See LL#11980 for 95 Preset menu access using KBD960 Keyboard.