Does the CM9760-KBD require any dip switch configuration to operate with the CM9700 Series Matrix Switcher?

Issue

Does the CM9760-KBD require any dip switch configuration to operate with the CM9700 Series Matrix Switcher?

Product Line

Pelco Matrix

Environment

CM9760-KBD
CM9700 Series Matrix Switcher

Cause

Installation / Configuration

Resolution

The CM9760-KBD-US does not require any physical addressing if it is being used with a CM9700 Series Matrix Switcher.
All programming is done through the software programming utility System Manager.

Refer to page 26 in CM9700-MGR Software Guide