Default IP address of the IP3701

Issue

What is the Default IP address of the IP3701?

Product Line

Pelco Cameras

Environment

IP3701

Cause

The camera automatically assign a static IP address when the DHCP server down.

Resolution

The network automatically assigns an IP address to the camera. The following scenarios describe how a DHCP or static network assigns IP settings:

  • DHCP network: If the camera is connected to a DHCP network, the server will automatically assign an IP address to the camera. DHCP is the default setting for the camera.
  • Static IP network: The IP address 192.168.0.20, on netmask 255.255.255.0, is automatically assigned to the camera.
     

If the camera has an older software version installed (version 01.00.0018 for IP3701H), the camera will automatically cycle through a range of IP addresses. The first available address found, 169.254.200.0 through 169.254.200.255 on netmask 255.255.0.0, will be assigned to the IP camera.