Does the CM9760-MDA pass coaxitron signals?

Issue

Does the CM9760-MDA pass coaxitron signals?

Product Line

Pelco Matrix

Environment

CM9760-MDA

Cause

The Master Distribution Amplifier is a 16-channel video distribution amplifier that distributes video to multiple devices without image degradation.

Resolution

The MDA does not pass Coaxitron® signals; however, the MDA can be used with Coaxitron products such as the CM6700, CM6800, and the CM9760-CXTA.

For setup illustration see page 54 and 55 of the CM9760-MDA Installation and Operation Manual