How are the CM9700 Matrix camera titles changed from the CM9760-KBD?

Issue

When using the CM9700-KBD, where do you change the camera titling?

Product Line

Pelco Matrix

Environment

  • CM97XX Large Matrix System
  • CM9760-KBD (any version)

Cause

Application requires camera labels.

Resolution

The camera titles cannot be modified from the CM9760-KBD.

To configure Camera label

  1. Load the Pelco System Manager (version must match the CM97XX-CC1 software) software on a Microsoft Windows PC.
  2. Import configuration files from the Matrix into the Pelco System Manager program using a floppy disk.
  3. Modify camera titles in the camera field using the Pelco System Manager program.
  4. Export configuration files from the Pelco System Manager program to the floppy drive.
  5. Reload the configuration files into the Matrix using a floppy disk.