How to setup alarm events to display on the Spot monitor on the DX4500/DX4600 Series hybrid video recorder (HVR).

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I setup event popup to display on the Spot monitor on the DX4500/DX4600 Series hybrid video recorder (HVR)?

Product Line

Pelco Video Management

Environment

  • DX4500 all versions
  • DX4600 all versions

Cause

Configure the Spot monitor to display an alarm event.

Resolution

The DX4500/DX4600’s spot monitor output can be used for public viewing or alarm call-up.

To configure the Spot monitor to display alarm popup:

  1. Go to Setup Menu
  2. Select Display
  3. Select Spot Monitor
  4. Select Event Popup > Alarm
  5. Close to Save