NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
DX4500/DX4600 USB Flash Drive Compatibility Report.
Product Line
Pelco Video Management
Environment
DX4500/DX4600 Series
Cause
Export video from DX4500/DX4600 Server.
Resolution
The report provides information about USB flash drives you can recommend for use with the DX4500 and DX4600 Series Digital Video Recorder. Product Support Engineering has tested the USB flash memory drives listed in the table below.
Note: The USB flash drives list in the table below were tested using the same backup/export test settings (listed next) and passed essential test criteria. The DX4500/DX4600 Linux operating system does not support USB drives capacities greater than 360GB.
Manufacturer/Model/Size | Export | Backup | If No, Explanation |
---|---|---|---|
Memorex, Travel Drive, 512 MB | Yes | Yes | |
Memorex, M-Flyer, 2 GB | Yes | Yes | |
LG, Xtick, 256 MB | Yes | Yes | |
SanDisk, Cruzer Titanium, 2.0 GB | Yes | Yes | |
HyperDrive, 8 GB | No | No | When inserted into the DX4500/DX4600, the USB drive reported "write protected" |
I/O magic, Gigabank, 12 GB | Yes | Yes | |
Imation, 2 GB | Yes | Yes | |
MXI ClipDrive, "Pelco Brand" 64 MB | No | No | Backup sample is too large since USB Disk is only 64 MB |
Staples, Relay, 2 GB | Yes | Yes | |
DiskGo, Edge, 1 GB | Yes | Yes | |
Sony, MicroVault, 4 GB | Yes | Yes | |
PNY, Attache, 4 GB | Yes | Yes | |
SanDisk, Cruzer Freedom, 1 GB | No | No | When inserted into the DX4500/DX4600, the USB drive reported "write protected" |
Maxtor, OneTouch 4 Mini, 160 GB | Yes | Yes | |
Toshiba, HDDR250E03X, 250 GB | Yes | Yes | |
Pelco "Endura" Brand, 1 GB | No | No | The disk cannot be formatted properly |
HP v125W, 2 GB | Yes | Yes | |
Western Digital, Passport Essential, 320 GB | Yes | Yes |