Where can I download the Spectra Mini manuals

Issue

Manuals and product literature can save time when installing and maintaining Pelco products.

Product Line

Pelco Cameras

Environment

Spectra Mini – All versions.

Cause

Installation and service.

Resolution

  1. To download product literature for the Spectra Mini series PTZ (Pan, Tilt, Zoom) cameras, browse to Pelco.com
  2. Type Spectra Mini in the search field located in the upper right hand of the page. See figure 1.
  3. Click on Pan/Tilt/Zoom (PTZ) Cameras. See Figure 1.
  4. Click on Indoor Surface Mount/In-Ceiling Miniature Dome System - Spectra Mini
  5. The Product page will load and display the Overview tab by default. Overview tab display product features. See Figure 2.
  6. Click on the Downloads TAB. See figure 3.
  7. Click on the Manuals BUTTON
  8. Under the DOC column; click on the pdf icons to download manuals. See Figure 3.

 


Figure 1: Search result for Spectra Mini

 


Figure 2: Spectra Mini page

 


Figure 3: Downloads tab in Spectra Mini page