Issue
Need to program and connect a KBD300A Universal Keyboard to a CM9700 Series Matrix Switcher.
Product Line
Pelco Matrix
Environment
KBD300A: Version 5.3 and above
CM9700: Version 9.03.***
Cause
Instructions are needed to program and connect a KBD300A Universal Keyboard to a CM9700 Series Matrix Switcher.
Resolution
- Open Pelco System Manager version 9.03.032 or greater.
- Log into the program using User/Password Admin/Admin using a capital "A"
- If the files need to be imported please use Lessons Learned Article #12916.
-
In the upper left hand corner select add device.
-
In the drop down menu select Data Translator and then Internal DT
-
Number of devices will be 1, select next.
-
Now enter the port number, baud rate 9600 and parity odd for the KBD300A
-
An operator will be added, this should not be changed, select next.
-
The new Internal DT (IDT) has now been created for the new KBD300A Universal Keyboard.
- You must export your files to disk and load them on the CM9700-CC1, use Lessons Learned Article #10699.
KBD300A Operation
Note: By default the KBD300A does not require a 4 digit login pin
- Connect the KBD300A to the CM9700-CC1. Connect a KBD300A to operate with a CM9700 Series Matrix Switcher using the figure below.
- Press 01 on the KBD300A then the Mon key or select the desired monitor. The display will only indicate which monitor is currently being controlled.
- Press the desired camera number on the KBD300A then press the Cam key to select the camera