Creating a Macro with the CM9700 System Manager with Version 9.03.032

Issue

How to create a Macro using System Manager Version 9.03.032?

Product Line

Pelco Matrix

Environment

CM9700 Version 9.03.***
CM9760 Version 9.03.***
CM9765 Version 9.03.***
CM9770 Version 9.03.***
CM9780 Version 9.03.***
CM9700 System Manager Software Version 9.03.032

Cause

Adding New Macros to the CM9700 System Manager Software

Resolution

To add a new Macro using the CM9700 System Manager Software, see section 'Adding a Macro' on page 50 in CM9700-MGR Software Guide.