CM9760-CDU-T Code Distribution Unit Addressing

Issue

Are the Sixteen 3-Position Screw Terminal Connectors on the CM9760-CDU-T addressable?

Product Line

Pelco Matrix

Environment

CM9700
CM9760
CM9765
CM9770
CM9780
CM9760-CDU-T

Cause

Addressing a CM9760-CDU-T

Resolution

The Sixteen 3-Position Screw Terminal Connectors on the rear panel of the CM9760-CDU-T are not addressable. Once the CM9760-CDU-T receives the address from the transmitter, the address is distributed to all 16 terminals on the CM9760-CDU-T.