How do I export the DS Media Player with the video using DS ControlPoint.

Issue

Require the DS Media Player to export with the video clip to a file.

Product Line

Pelco Video Management

Environment

  • DS Control Point version = All
  • DS Media Player
  • IMedia.exe
  • Digital Sentry

Cause

The DS ControlPoint software is able to export a video clip in the native format as well as the DS Media Player into a single file (EXE).

Resolution

EXPORTING TO A NON-CD/DVD LOCATION

To export video included from a search result to a location on your hard drive (non-CD/DVD), complete the following steps:

  1. Click the Export icon
  2. On the Export tab, select Video and click the Next button.
  3. Select EXE (if not selected) to include the DS Media Player and click the Next button.


     
  4. Click the Browse button to select the name and location for the export file, and then click the Next button.
  5. Select the streams to export. In this tab, you can select Select All or Clear All, and then click the Next button.
  6. Use the status bar slider to select the beginning of the search result that you want to export, and then click the Next button.
  7. Use the status bar slider to select the end of the search result that you want to export, and then click the Next button.

The export begins and the status bar shows the progress of the export. Once the export is completed, the search option screen will reappear.