Spectra IV Power Up Mode option missing

Issue

Does the DD4CBW23 have a Power Up Mode option.

Product Line

Pelco Cameras

Environment

  • Spectra IV
    • DD4CBW23
    • DD423

Cause

"Power Up Mode" option not available on older models 

Resolution

The "Power up mode" option is available on the Spectra IV SE models or 27x and higher.

Option 

  1. Set the Park Time Action on the spectra dome. 
  2. If power is lost and the Spectra is facing a non-desire location each spectra will have to be moved slightly to activate the Park action mode.

Note: No other resolution available.