Options for adding new monitors and cameras to CM9760 Matrix Series system.

Issue

Since the CM9760 Matrix Series system is obsolete, what are the options for adding new monitors and cameras to the CM9760 system?

Product Line

Pelco Matrix

Environment

CM9760 Series Matrix Switcher / Version 7.00.000 -.8.03.012


CM9700 Series Matrix Switcher / Version 9.03.***

CM9760-VCC

CM9760-VMC

CM9760-MXB

CM9760-RPC

CM9760-RPL

CM9760-DFL

Cause

The CM9760 Series Matrix Switcher is obsolete

Resolution

The CM9760 Matrix Switcher will need to be upgraded to version 9.03.***

To upgrade your Matrix switcher to the latest version, please select and complete the CM9700 Upgrade application.

CM9700 Upgrade

Once the Matrix Switcher is upgraded to version 9.03.0XX,  the CM9765, CM9770 or CM9780-MXB matrix bay can be used to add the new monitors and cameras.