Compatible CM6700 Matrix Keyboards

Issue

What controller can be used with the CM6700?

Product Line

Pelco Matrix

Environment

CM6700
KBD100
KBD200
KBD300

Cause

Compatible Keyboards

Resolution

The KBD100, KBD200A, and KBD300A keyboards have been engineered for use with the CM6700 matrix switcher.
Each keyboard in the series offers a different level of control and functionality in order to provide maximum versatility in every application.