Programming Limit Stops on a Spectra Mini

Issue

How do I set scan limit stops on my Spectra IP Mini.

Product Line

Pelco Cameras

Environment

Spectra Mini / Version (all)
Spectra

Cause

Program stops that limit the pan range of the Spectra Mini

Resolution

LIMIT STOPS: Limit stops are programmable stops that limit the pan range of the dome. There must be two
limits, a left and a right, to define an area.

 There are two types of limit stops:

  • MANUAL - A manual (joystick) pan operation stops when a limit stop is reached.
     
  • SCAN - The dome reverses direction during random, frame, or auto scanning when a limit stop is reached.

 

To set manual or scan stops:

1. Use the joystick to position the cursor beside SET MANUAL STOPS or SET SCAN STOPS.
2. Press Iris Open.
3. Follow the directions displayed on the monitor.

NOTE: In order for the manual or scan stops to work, the LIMIT STOPS setting must be ON.

To clear manual or scan stops:

1. Use the joystick to position the cursor beside CLEAR MANUAL STOPS or CLEAR SCAN STOPS.
2. Press Iris Open.
3. Follow the directions displayed on the monitor.

NOTE: For additional programming, refer to Spectra Mini Operation and Programming Manual.