Issue
Spectra Lite * Spectra II * Spectra III * and Spectra IV Compatibility
Product Line
Pelco Cameras
Environment
All Spectra integrated systems – all models – all versions.
Cause
Over time the Hardware and firmware of the spectra integrated dome series has changed. Therefore some interface compatibilities will have changed also.
Resolution
The chart below gives information on which dome drives fit into which back box housings.
Spectra Integrated Positioning Systems Compatibility Chart
Housing Back Boxes | ||||
Dome Drives | Spectra Lite | Spectra II | Spectra III | Spectra IV |
Spectra/Lite DD5 | X | |||
Spectra II DD5 | X | |||
Spectra III DD53 | X | X | X* | |
Spectra IV DD4 | X* | X |
Spectra Series backbox
- BB5: Spectra
- BB5A: Spectra II
- BB53: Spectra III
- BB4: Spectra IV
* The Spectra III and IV have a heat transfer incompatibility and if used in outdoor applications may present integrity risk.
Spectra IV Product Page - https://www.pelco.com/video-surveillance-camera-security-systems/analog