Can I use the FS85011AMST or FS85011ASST in the Pressurized Spectra IV?

Issue

Can I use the FS85011AMST or FS85011ASST in the Pressurized Spectra IV?

Product Line

Pelco Transmission & Power

Environment

FS85011AMST
FS85011ASST
BB4-PRM-E
BB4-PRS-E

Cause

Customer did not order the correct model or was shipped the incorrect model of pressurized Spectra IV fiber connector on the FS85011AMST or FS85011ASST would not connect through the back box of the Pressurized Spectra IV.

Resolution

The back box that will work with the FS85011ASST is BB4-PRM-E and the correct back box that will work with the FS85011ASST is BB4-PRS-E. The dome drive and lower dome will work with the replacement back box.