Programming a CM9760-CXTA to System Manager Version 9.03.032

Issue

Add a CM9760-CXTA to a CM9700 Matrix Switcher.

Product Line

Pelco Matrix

Environment

CM9700-CC1 version 9.03
Pelco System Manager version 9.03.032
CM9760-CXTA

Cause

Additional cameras with Coaxitron Control need to be added.

Resolution

PART I:  ADDING THE CM9760-CXTA

1. Click on the Add Device Wizard

2. Select Device Type:  Click the drop-down box and choose Coaxitron then click the Next button


3. Number of Devices: Select the number of these devices to add to this CC1 node.  Select 1 then click the Next button


4. Port Configuration:  Select the host port.  In this example we are connecting the CM9760-CXTA to CM9700-CC1 sercom port 7.  The preferred default Baud Rate is 4800 and the parity is Even



5. Add More Devices?:  Click the Finish button


6. The CM9760-CXTA is now added to the device tree on sercom port 7


Part II:  ADDING A CAMERA TO THE CM9760-CXTA

1. Click on the Camera Tab
2. Click in the Port field and enter 7. This is the CM9700-CC1 sercom port number.
3. Click in the Address field and enter 1.  This corresponds with the BNC on the CM9760-CXTA.  In this example we are connecting the PTZ camera to CM9760-CXTA BNC 1.


 

For instructions with illustration, download CM9700-MGR Software Guide.