What Pelco fiber transmitter and receiver will work with the Spectra HD high definition IP dome system?

Issue

What Pelco fiber transmitter and receiver will work with the Spectra HD high definition IP dome system?

Product Line

Pelco Transmission & Power

Environment

S5118-FW0
S5118-FW1
S5118-YB0
S5118-YB1
S5118-PG0
S5118-PG1
S5118-PB0
S5118-PB1
S5118-EG0
S5118-EG1

FMCI-PG Series

Cause

Specification Sheet for the Spectra HD high definition IP dome system lists no option for Pelco fiber transmitters and receivers.

Resolution

Below is a list of fiber transmitters and receivers that may be used with the Spectra HD high definition IP dome system.

For Single Port, 10Base-T/100Base-TX and Single Port 100Base FX Media Converter
FT82011MSTR-1 and FR82011MSTR-1 with multimode fiber ST connector; or the FT82011MSCR-1 and FR82011MSCR-1 Multimode SC connector.
FT82011SSTR-1 and FR82011SSTR-1 with Single mode fiber ST connector; or the FT82011SSCR-1 and FR82011SSCR-1 Single mode and SC connector.

FMCI-PG Series Media Converters (Requires FSFP Module)