Wiring the VERIFACT A microphone to the AUD-1 for a Sarix IP camera.

Issue

Wiring the VERIFACT A microphone to the AUD-1 for a Sarix IP camera.

Product Line

Pelco Cameras

Environment

  • Sarix (all models that use the AUD-1)
  • AUD-1

Cause

No information is in the manual with reference to the VERIFACT A 3 wire microphone.

Resolution

Please follow the wiring instruction listed below to connect the Verifacta 3 wire microphone to the AUD-1